Configure firewall for an OPC UA server
    If an application has an OPC UA server running in Windows®, open the port specified in the 
Endpoint URL Server
 property of the OPC UA server.Prerequisites
- To configure firewall for an OPC UA server
- When running a project with an OPC UA server object, if prompted, accept requests to configure a firewall rule.
The 
firewall rule is created.runtime
Provide Feedback