Export nodes to NodeSet
    Export nodes to a NodeSet 
XML
 file. Use the exported file to exchange OPC UA Companion Specifications
.Prerequisites
Add nodes to the project. See Project nodes.
- To export nodes to NodeSet
- InProject view, right-click a node to export and selectExport to NodeSet.TIP: You cannot export the root project node.
- Select a location for the NodeSetXMLfile.The selected node and child nodes are exported.
- (optional) In the export notification, selectOpen containing folderto navigate to the exported NodeSetXMLfile.
Import the NodeSet to an OPC UA server, another 
FactoryTalk Optix
 project, or browse the nodes offline in an OPC UA client.Provide Feedback