Delete an event logger
    Delete an event logger by removing the event logger object in 
Project view
.
     TIP: 
    You can disable an event logger without the need to completely remove the logger from the project. For more information, see Edit an event logger.
- InProject view, right-click an event logger object and selectDelete.
Provide Feedback