Store read operation codes
    Configure the logger to store the operation codes of reading on the controller in the database.
     TIP: 
    For more information about the read operation codes, see Read operation codes.
Prerequisites
- To store read operation codes
- InProject view, select a data logger object.
- InProperties, setLog operation code of each variabletoTrue.
operation code
    
Provide Feedback