Delete a template
    Delete a template from a library that you no longer need.
- From the main toolbar, select.Template Libraries
- Select a library or a library folder that contains the template to delete.TIP: You can also use search to locate the template. See Search for a template.
- UnderComponents, select a template to delete.
- Next toComponents, select.Delete
- SelectYes.
Provide Feedback