Libraries
    Libraries contain object definitions that you can add to your projects.
Library types
      
  | Type | Description | 
|---|---|
| Template library | The default library of objects that you cannot edit or remove. Template libraries are provided for:
                   
 | 
| Custom library | A library created by a user that contains a set of objects either curated from the template libraries or customized for specific automation scenarios. | 
     TIP: 
    To find a template quickly, select any item under 
Components
 and start typing.Library repositories
      You can store libraries locally or in a remote Git repository. Libraries are available across 
FactoryTalk Optix
 projects.Libraries are saved in the  folder.
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\LibrariesLibrary updates
      Libraries and library objects are tied to the version of the 
FactoryTalk Optix
 software with which they were originally configured. When you install an updated version, FactoryTalk Optix
 updates the built-in template libraries to make the libraries compatible with the new software.If your project contains custom libraries that use components that changed in the updated version of 
FactoryTalk Optix
, you must manually update the custom libraries.library
    
Provide Feedback