Configure a style sheet
    Set 
Global Style
 to edit the styles applied to all graphic objects. Set Control Styles
 to edit the styles applied to specific control objects. Control styles overwrite the global style.- InProject view, select the style sheet to edit.TIP: You can select the default style sheet, add a predefined style sheet, or create your own style sheet. See Add a predefined style sheet or Create a style sheet.
- To set the global style that applies to all graphic objects, inProperties, underGlobal Style, selectand enter the values. TIP: You can create dynamic links instead of entering the values manually. See Create dynamic links. TIP: You can create dynamic links instead of entering the values manually. See Create dynamic links.
- To create a control style, underControl Styles, next to, selectObjectstyles. For example, create a control style for switch objects. For example, create a control style for switch objects.
- To rename a control style, hover-over the style name, selectand enter a new name. 
- To edit a control style, expand, expand the style name, and then edit the properties by selectingObjectstylesand entering values. TIP: You can also create dynamic links instead of entering the values manually. See Create dynamic links. TIP: You can also create dynamic links instead of entering the values manually. See Create dynamic links.
- To delete a control style, next to the style name, select.Delete
Provide Feedback