Advanced SVG image
    Use this object to display an SVG Tiny 1.2 image and change the properties of individual image parts at design time or runtime.The SVG image must contain the ID attribute and properties for the individual image parts you want to change.
Application example - disabled alarm

Application example - enabled alarm

Use case
      Statically or dynamically modify a part or the entire SVG image. For example, signal a hardware part malfunction by highlighting a given hardware component representation.
Provide Feedback