Screen
    Use screens to group objects that comprise a specific interface.
Screen types and instances
      For optimal project maintainability, create screen object types and then use them with panel loaders or navigation panels. This allows you to modify all screen instances by editing the parent screen type.
Screens folder
      Rockwell Automation
 recommends creating screen types in the  folder in Project view
. You can also create screen types in different nodes of your project, for example in the UI folder.Each new project contains an empty 
    
    
Screens
 folder.
        
     TIP: 
    If the project does not contain a 
Screens
 folder, see Add a Screens folder.Provide Feedback