Popup
    A window that displays when an event is triggered.
Use case
      You can use popups for error handling, confirmation messages, or status notifications.
Example
      A popup that displays when the Toggle Popup button is pressed

Provide Feedback