Panel
    Container for objects. By default, each new panel has a fixed width and height and is aligned with the top-left corner of the parent object.
Example
      ColorPicker1 Panel and children objects

ColorPicker1 Panel in the editor

Provide Feedback