Linear gauge
    Sets or displays an integer value within a range of possible values.
Use case
      Set or display the value of an analog variable within a minimum and maximum value.
        
    
    
     TIP: 
    Use the 
Tooltip
 property to show or hide the display of the value above the selection point on the gauge. Use the Warning zone
 property to display specific ranges of values in different colors.Example
      Linear gauge with two warning zones defined

Provide Feedback