Label
    Displays text that describes an item.
Use case
      Display static or dynamic text. For example, display the value of a variable in real time or the name of the currently logged in user.
        
    
    
     TIP: 
    To display dynamic text, create a dynamic link between the 
Text
 property and a variable. Use a String formatter to customize the displayed variable value.Example
      
Provide Feedback