References to dynamic link sources
    Depending on the type of a dynamic link source, the property value field displays the reference in different ways.
Property values
      
  | Source type | Property value | 
|---|---|
| A node or a variable | The  BrowseNameof the source. | 
| An attribute of a node or of a variable | BrowseName@ name of the attribute | 
| An array variable | BrowseName[ array index values] | 
| An array index of the array variable | BrowseName[ array index number] For example,  [0]is the first array index. | 
| A bit index  | BrowseName[ bit index number] 
                For example, [0] is the first bit index. | 
| A property of a node | The path to the source node. | 
| A node or a variable formatted by the user | The information about the source followed by  (formatted) | 
| Reference type | Description | Property value example | 
|---|---|---|
| Absolute | A complete path to the referenced source that starts with the root directory. | ProjectName/Model/SourceVariable | 
| Relative | A path to the referenced source that starts with the target node directory. | ../SourceVariable | 
| With aliases | Any type of a path that contains aliases. An alias is a variable type that points to a source node and has a unique identifier property. For more information, see Aliases. | {Motor}/Speed | 
     TIP: 
    
Selecting the blue link (
../SourceVariable
 in the example), brings you to the link target (SourceVariable
 node).
Provide Feedback