SQL queries
    SQL (Structured Query Language) manages data stored in relational databases through simple, declarative statements. Use the ANSI SQL-92 standard for querying ODBC databases and embedded databases.
SQL grammar
      The top-down SQL parser is based on a simplified version of standard SQL grammar because:
        
- FactoryTalk Optix supports only a subset of standard SQL.
- The simplified standard SQL grammar best fits to the top-down parser implementation.
- The simplified standard SQL grammar facilitates the readability of the resulting AST.
Statements
      FactoryTalk Optix Studio
 supports these statements in SQL queries:
        - Use theSELECTstatement to select data from a database. This statement supports both column names and value expressions, as well as theALLandDISTINCTset quantifiers.Examples:SELECT *, FROM Table1 SELECT *, Timestamp AS T FROM Table1 SELECT Column1 FROM Table1 SELECT *, 10 FROM Table1 SELECT 10, * FROM Table1 SELECT *, 'text value' FROM Table1 SELECT COUNT(*) FROM Table1 SELECT DINSTINCT Column1 FROM Table1NOTE: TheCASEandWHENexpressions are not supported.IMPORTANT:The SQL standard does not allow combining*with derived columns.SELECT *, Timestamp FROM Table1SELECT *, ROW_NUMBER() OVER (ORDER BY Timestamp) FROM DataLoggerFactoryTalk Optixsupports this standard to allow any query manipulation for Sparkline charts.
- Use theDELETEstatement to delete any existing records in a table.Examples:SELECT * FROM Table1 WHERE ... DELETE FROM Table1 WHERE ... UPDATE Table1 SET column1 = 10 WHERE column2 > 20 ...
- Use theUPDATEstatement to modify any existing records in a table.Examples:SELECT * FROM Table1 WHERE ... DELETE FROM Table1 WHERE ... UPDATE Table1 SET column1 = 10 WHERE column2 > 20 ...
FactoryTalk Optix Studio
 partially supports these statements in SQL queries:
        - Use theCREATEstatement to create tables or tables in databases. This statement partially supportsTABLEandINDEX.Examples:CREATE UNIQUE INDEX Table_Index ON Table1 (Column1) CREATE INDEX IF NOT EXISTS Table_Index ON Table1 (Column1)CREATE TABLE TempTable AS SELECT Column1 FROM MyTable WHERE Column1 > 5 CREATE TEMPORARY TABLE TempTable AS SELECT Column1 FROM MyTable WHERE Column1 > 5CREATE TEMPORARY TABLE Table2 AS SELECT Column1 FROM Table1 WHERE Column1 > 5 CREATE UNIQUE INDEX Column1_Index ON Table1 (Column1) DROP TABLE Table1
- TheDROPstatement drops any existing databases or tables in databases.Examples:DROP TABLE TemporaryTable DROP TABLE Table1
Literal values
      
  | Literal value type | Example | Notes | 
|---|---|---|
| Integral | 1520 | Do not use thousands separators. Use the Int32 type. | 
| Real | 15.025 | Use  .as the decimal separator. Use the Double type. | 
| Real scientific | 2.7000001072883606E-1 | |
| Boolean | 
 | Use lowercase for Boolean values. | 
| String | 'string value' | Use single quotes to delimit text. Insert a single quote ( ') in a text string by escaping the single quote with another single quote. For example, to write 'string', use two single quotes ''string''in the strings. | 
| Date and time | "2004-05-23T14:25:10.487" | Use the ISO8601 format delimited by double quotes. The date and time notation is non-standard ANSI SQL used to avoid the DATE, TIME, and TIMESTAMPkeywords without ambiguity. | 
| Regular identifier | 
 | Do not use spaces. Start with an uppercase or a lowercase letter. You can use numeric digits, letters, and the underscore character  _. | 
| Delimited identifier | 
 | Use double quotes ( ") as the delimiter. In the identifier, use any character except for the  "character. Any spaces at the end of the identifier are ignored. | 
Join
      Any kind of joins such as 
    
INNER
, UNION
, LEFT
, RIGHT
, FULL
, NATURAL
 and CROSS
 is supported.
        
     NOTE: 
    Some joins are not fully supported by every DBMS.
Aliases
      You can use aliases in the identifiers, derived column subqueries, and tables.
The following are examples of queries with aliases:
        
SELECT Timestamp AS T FROM Table1 WHERE ...
SELECT * FROM Table1 AS T WHERE ...
SELECT * FROM (SELECT * FROM Table1) AS SubQuery WHERE ...
CREATE TABLE Table1 AS SELECT Timestamp, Column1 FROM Table2
Table references
      The 
FROM
 clause supports the following table references.| Reference | Example | 
|---|---|
| Fully qualified reference | ... FROM table_name ... FROM schema_name.table_name ... FROM database_name.schema.name.table_name | 
| Sub query | ... FROM (SELECT * FROM Table2) WHERE ... | 
     NOTE: 
    Fully qualified names are also supported as column references.
Examples:
        
... WHERE Table1.Column1 > 10... WHERE Table1."order id" > 10 SELECT * FROM Table1 AS T WHERE T."order id" > 10 ... WHERE "my table"."order id" > 10
Operators
      
  | Operator | Example | 
|---|---|
| IN | 
 | 
| BETWEEN | 
 | 
| LIKE | 
 
 
 | 
| EXISTS | 
 | 
| IS | 
 | 
| NOT | 
 
 
 The  NOToperator applies to all other operators. | 
     NOTE: 
    
ANY
 and ALL
 operators are not supported.Window functions
      
  | Function | Example | 
|---|---|
| ROW_NUMBER | 
 
 
 | 
| RANK | 
 | 
| DENSE_RANK | 
 | 
| AVG | 
 | 
| SUM, MIN, MAX | 
 | 
| COUNT | 
 
 | 
     NOTE: 
    The 
PARTITION BY
 clause supports only column identifiers.Tokens
      
  | Token | Regular expression | 
|---|---|
| regular_identifier | [a-zA-Z][a-zA-Z0-9_]* | 
| delimited_identifier | ".*?" | 
| real | |
| boolean | |
| Other trivial tokens | Regex for single char or single-word tokens | 
     NOTE: 
    The lexer does not recognize date and time values as tokens: they are parsed as 
delimited_identifier
. The semantic analyzer extracts any date and time values from the delimited_identifier
 according to the r
 regular expression.Provide Feedback