OMRON EtherNet/IP driver
    Observe these guidelines when working with the OMRON EtherNet/IP driver.
Supported controllers
      The driver may support these controller families:
        
- OMRON® NJ Series
- OMRON® NX Series
- OMRON® NU Series
     IMPORTANT: 
    The driver has been tested with NJ301-1100 firmware revision 1.09 and NJ101-9000 firmware revision 1.50.
Controller tags import
      You can only import tags from 
TXT
 files in the offline mode.
     IMPORTANT: 
    
Before importing tags:
          
- In Sysmac® Studio, setNetwork PublishtoPublish only.
- From Sysmac® Studio, export tags to aTXTfile.
For more information, refer to the product documentation.
Data types
      The driver supports these data types:
        
  
    
| Controller data type | FactoryTalk Optixdata type | Length | Notes | 
|---|---|---|---|
| BOOL | BOOL | 1 BIT | |
| BYTE | BYTE | 1 BYTE | |
| WORD | UINT16 | 2 BYTES | |
| DWORD | UINT32 | 4 BYTES | |
| LWORD | UINT64 | 8 BYTES | |
| SINT | SBYTE | 1 BYTES | |
| INT | INT16 | 2 BYTES | |
| DINT | INT32 | 2 BYTES  | |
| USINT | BYTE | 1 BYTE | |
| UINT | UINT16 | 2 BYTES | |
| UDINT | UINT32 | 4 BYTES | |
| LINT | INT64 | 4 BYTES | |
| ULINT | UINT64 | 8 BYTES | |
| REAL | FLOAT | 4 BYTES | |
| LREAL | DOUBLE | 8 BYTES | |
| TIME | DURATION | 4 BYTES | |
| DATE | DATE TIME | 2 BYTES | Use these data types with  Date and timeobjects, which allow you to set and view date and time data. | 
| TIME_OF_DAY(TOD) | UTC TIME | 4 BYTES | |
| DATE_AND_TIME(DT) | DATE TIME | 8 BYTES | |
| STRING(256) | STRING-MAX256 | 256 BYTES | |
| ARRAY 1 dimensional | Type [dimension] | ||
| ARRAY 2 dimensional | Type [1st dimension, 2nd dimension] | ||
| ARRAY 3 dimensional | Type [1st dimension ,2nd dimension, 3rd dimension] | 
Provide Feedback