Micro Controller Driver
    Observe these guidelines when working with Micro Controller Driver.
Supported controllers
      Micro Controller Driver supports 
Micro800™
 controllers and MicroLogix™
1400 controllers.Controller tags import
      With Micro Controller Driver, you can import tags from 
Micro800
 controllers in the online mode.Data types
      Micro Controller Driver supports these data types:
| Datatype  | FactoryTalk Optixdatatype | 
|---|---|
| BOOL  | Boolean | 
| SINT  | SByte  | 
| DINT  | Int32  | 
| REAL | Float  | 
| STRING  | String  | 
| LREAL  | Double | 
| INT  | Int16  | 
| LINT  | Int64  | 
| USINT  | Byte  | 
| BYTE  | |
| UINT  | UInt16  | 
| WORD  | |
| UDINT  | UInt32  | 
| DATE  | |
| TIME  | |
| DWORD  | |
| ULINT  | UInt64 | 
| LWORD  | 
Provide Feedback