Translate an alarm message
    The message displayed in an 
Alarms
 widget is a text string that can appear in different languages. Enter a message, select the language for the translation, and then enter the translated string. The translated alarm message appears in the language of the user at runtime.Prerequisites
- To translate an alarm message
- InProject view, navigate to and select the alarm.
- InProperties, inMessage, type the message the alarm event is to display at runtime.
- InProject view, expandTranslations.
- Double-clickLocalizationDictionary#
- In the Translation Editor, selectViewTranslation Reference.Your new message appears in theStringcolumn.
- In the row of the alarm message, select Synchronize.A corresponding translated message appears in theKeycolumn. Synchronize.A corresponding translated message appears in theKeycolumn.
- SelectView Translation Table.
- SelectAdd locale, select the desired language for the translation, and then select. 
- InNew locales added, selectYes.
- In the third column, enter the string for the translation.
locale
localize
synchronize
translate
    
Provide Feedback