View alarms in UTC time zone
    Alias the 
Time
 property of the Alarm grid
 object to view events in the UTC (Coordinated Universal Time) time zone standard. UTC is the time standard on which all time zones are based worldwide. Viewing alarms in the UTC time zone ensures that all users are seeing the same time stamps for the alarms. - In the main toolbar, select.Template Libraries
- InTemplate Libraries, selectWidgets.
- Drag theAlarms Gridobject to the desired folder in theUIfolder.AlarmGrid# (type)appears.
- InTemplate Libraries, selectClose.
- In the editor, select the alarm grid and then inProperties:- ExpandTimestamp.
- Expand theData gridcategory.
- Expand theColumncategory and then selectDataItemTemplate.
- InText, select. Add Dynamic Link Add Dynamic Link
- In theDynamic Linkswindow, expandAliases.
- ExpandAlarm Conditionand then selectTime.
- ChooseSelect.
 
alarm history grid
local time
time zone
    
Provide Feedback