Develop a button that animates an SVG image

Configure an Advanced SVG Image object to animate the image at runtime.
NOTE:
Download a sample project:
RotateImage.zip
Application example
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal