Known anomalies in this release

The list identifies the known anomalies in
FactoryTalk Optix
version 1.3.x.
Use the identification information in parenthesis to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
Compute Module with multiple backplanes in controller path unable to communicate with controller
The Compute Module cannot communicate with the controller if there is more than one Backplane in the controller path. For example, the module is unable to communicate with the controller if the path is Backplane\1\A\10.220.173.66\Backplane\3. However, paths resembling either Backplane\3 or Backplane \1\A\10.220.173.66 allow the module to communicate with the controller. 
This anomaly first identified in version 1.2.0.
Image does not appear at runtime (3140280)
If an image file in a project does not appear in the runtime application, use a third party application to resize the image and make it smaller.
This anomaly first identified in version 1.3.0.
Unable to export file when name of project contains special characters [3110366]
Filenames cannot contain special characters.
This anomaly first identified in version 1.3.0
No error appears when misconfiguring a string as a Discrete Input for a Modbus Station and all other tag reads fail (2351429)
Assigning a string tag to a Discrete input memory area does not display an error message and causes read errors on all tags for the Modbus Station containing the misconfigured tag.
This anomaly first identified in version 1.3.0.
Renaming a user-defined library using OneDrive may result in synchronization errors (2348900)
OneDrive is not recommended for storing user-defined libraries and may result in synchronization errors and duplicate files when renaming libraries. If attempting to use OneDrive to rename a library, unlink OneDrive when renaming the library. To unlink OneDrive, see Turn off, disable, or uninstall OneDrive.
This anomaly corrected in version 1.5.0.
This anomaly first identified in version 1.3.0.
Sparkline range cannot display if only one range is modified [3153055]
If you modify only the value for Range high or Range low for a sparkline, the range cannot display in sparkline. Modify both the value in Range high and Range low to display the range in the sparkline.
This anomaly corrected in version 1.4.0.
This anomaly first identified in version 1.3.0.
Custom library elements do not appear without restarting FactoryTalk Optix (2371413)
Elements added to a custom library do not appear in Libraries search until you restart
FactoryTalk Optix
.
This anomaly first identified in version 1.3.0.
Unable to launch FTOptixRuntime.exe [3187395]
FTOptixRuntime.exe cannot launch if you export the project to a folder with a name that contains a special character.
This anomaly corrected in version 1.4.0.
This anomaly first identified in version 1.3.0.
Unable to emulate a project [3196019]
The Emulator cannot run a project that contains a Rockwell Automation EtherNet/IP station if FactoryTalk Optix Studio is installed in a folder that contains a special character.
This anomaly corrected in version 1.4.0
This anomaly first identified in version 1.3.0
Video support may lag in some Windows DirectX configurations [3251408]
Setting the environmental variable FTOPTIX_RHI_BACKEND to "opengl" may resolve this issue.
This anomaly corrected in version 1.4.0
This anomaly first identified in version 1.3.1.
Special characters not always supported (2123530)
Special characters are supported in PDF filenames and FTP Server usernames, but are not supported when using the Microsoft Pinyin input method on the device.
This anomaly corrected in version 1.5.0.
This anomaly first identified in version 1.2.0.
Unable to deploy to device with invalid name [2239099]
Deploying to a device with a name that contains a slash results in an error or the application not running on the device.
This anomaly corrected in version 1.4.0.
This anomaly first identified in version 1.2.0.
Some videos may not play on computers running Microsoft Windows (2212837)
If you emulate a project on a computer that is running Microsoft Windows, some videos may not play. Videos will play if you deploy the project to a device.
This anomaly first identified in version 1.1.0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal