- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Security modes
Security mode for the Wi-Fi interface (WPA2-Personal/WPA2-Enterprise).
- BrowseName
- SecurityModeEnum
Values
Value | DisplayName | Description |
---|---|---|
0 | WPA2-Personal | WPA2-Personal mode. Username is not required. |
1 | WPA2-Enterprise | WPA2-Enterprise mode. Username is required. |
Provide Feedback