Global methods for UI

This method impacts the user interface.

OpenDialog method

This method opens the dialog window object that is set as an argument.
Input arguments
Argument
Description
Dialog
Dialog window to open.
AliasNode
Alias that identifies the data model of the contents to be shown in the dialog
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal