Runtime method types

Methods are executed at runtime when an event occurs.

Local runtime methods

Local methods are exposed by project objects, including:
  • Alarms
  • Loggers
  • Databases
  • Graphical objects
For example,
Video
objects expose the
Play
method that starts the video playback.

Global runtime methods

FactoryTalk Optix Studio
exposes global methods regardless of the selected node. Global methods are divided into these categories:
  • Variable commands
  • Core commands
  • Alarm commands
  • UI commands
  • Recipe commands
For example, the
Acknowledge all
method acknowledges all alarms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal