Scale line pen

XY chart object pen that draws a line whose points represent the X and Y coordinates of two variables X and Y.
BrowseName
XYChartScalarLinePen
SuperType
XY chart line(XYChartLinePen)

Properties

Name
BrowseName
DataType
Description
X
X
X coordinate variable.
Y
Y
Y coordinate variable.
Color
Color
(Inherited from XY chart line)
Thickness
Thickness
(Inherited from XY chart line)
Enabled
Enabled
(Inherited from XY chart pen)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal