Polygon pen

XY chart object pen. Draws a line whose values represent both dimensions of a two-dimensional matrix variable and links the first and last point drawing a polygon.
BrowseName
XYChartPolygonPen
SuperType
XY chart pen(XYChartPen)

Properties

Name
BrowseName
DataType
Description
Point array
PointArray
Bidimensional array of X, X coordinates that should be drawn by the chart.
Fill color
FillColor
Fill color of the polygon area.
Border color
BorderColor
Color of the polygon border.
Thickness
Thickness
Weight of the pen line.
Enabled
Enabled
(Inherited from XY chart pen)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal