Array line pen

XY chart object pen that draws a line whose points represent both dimensions of a two-dimensional matrix variable.
BrowseName
XYChartArrayLinePen
SuperType
XY chart line(XYChartLinePen)

Properties

Name
BrowseName
DataType
Description
Point array
PointArray
Bidimensional array of X, X coordinates that should be drawn by the chart.
Editable
Editable
Enable/disable the change of the value directly in the chart.
Color
Color
(Inherited from XY chart line)
Thickness
Thickness
(Inherited from XY chart line)
Enabled
Enabled
(Inherited from XY chart pen)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal