Value axis

Y axis of the values of a Trend Graph.
BrowseName
ValueAxis
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Minimum value
MinValue
Minimum value displayed on the Y axis.
Maximum value
MaxValue
Maximum value displayed on the Y axis.
Automatic scaling
AutoScale
Enable/disable resizing of the Y axis based on the minimum and maximum values displayed in the graphic at runtime.
Interactive
Interactive
Enable/disable interactivity with the axes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal