Switch

Set and display a Boolean value.
BrowseName
Switch
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Checked
Checked
Interrupter status. To enable another interface object when the value is True, create a dynamic link between this property and the Enabled property of the object to be enabled.
Text shown if on
CheckedText
Text displayed inside the object when Active = True.
Text shown if not on
UncheckedText
Text displayed inside the object when Active = False.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

Modified value
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal