Scroll view

Panel with the possibility of scrolling, to display content larger than the panel itself.
BrowseName
ScrollView
SuperType
Container(Container)

Properties

Name
BrowseName
DataType
Description
Enables zoom
Zoommable
Enable pinch-to-zoom.
Maximum zoom in
MaxZoomIn
Magnification limit in percent.
Minimum zoom out
MinZoomOut
Shrinkage limit in percent.
Scroll axes enabled
ScrollAxesEnabled
Axes for which scrolling is enabled.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal