ScrollBar style

Global properties for all project scroll bars.
BrowseName
ScrollBarStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
ScrollBar auto hide
AutoHide
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Size
Size
Handle color
HandleColor
Handle border color
HandleBorderColor
Handle border width
HandleBorderWidth
Handle radius
HandleRadius
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal