Panel
Simple objects container. Display the graphical objects it contains and that can be a selectable area.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Hit test visible | HitTestVisible | True = intercept user clicks. False = does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis. | |
Provide Feedback