Number animation

BrowseName
NumberAnimation
SuperType
Abstract animation(AbstractAnimation)

Properties

Name
BrowseName
DataType
Description
From
From
Start value of the range.
To
To
Final value of the range.
Duration
Duration
Duration of the animation in milliseconds.
Interpolation
EasingCurve
Defines the interpolation distribution used for animating the value change.
Target
Target
Running
Running
(Inherited from Abstract animation)
Loops
Loops
(Inherited from Abstract animation)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal