Search
FactoryTalk Optix Studio Help Center
Navigation panel style
Global properties for all project Navigation panel objects.
BrowseName
NavigationPanelStyle
SuperType
Control style
(ControlStyle)
Properties
Name
BrowseName
DataType
Description
Color
InactiveColor
Color
Color of the range.
Inactive text color
InactiveTextColor
Color
Active color
ActiveColor
Color
Active text color
ActiveTextColor
Color
Background color
BackgroundColor
Color
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Font family
FontFamily
Font
Font family.
Font weight
FontWeight
Font weight
Font weight.
Font italic
FontItalic
Boolean
Enables/disables italics in the text.
Font size
FontSize
Size
Font size.
Radius
Radius
Size
Radius of the angles of the objects.
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal