Image

Display an image.
BrowseName
Image
SuperType
Container(Container)

Properties

Name
BrowseName
DataType
Description
Path
Path
Path.
Dynamic color
DynamicColor
(For SVG formats only) Replace the colors of the image with the selected color (RGB) in the way specified in Colorization Mode. The alpha channel of the color is ignored. SVG elements that do not have a color specified and do not inherit a color appear black.
Fill Mode
FillMode
Fill mode of the image object (Fit = resize the image keeping the original aspect ratio, Stretch = resize the image by fitting the aspect ratio to the area of the image object).
Hit test visible
HitTestVisible
True = intercept user clicks. False = does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis.
Image left margin
ImageLeftMargin
Size of the left peripheral section to exclude from the image resizing.
Image top margin
ImageTopMargin
Size of the top peripheral section to exclude from the image resizing.
Image right margin
ImageRightMargin
Size of the right peripheral section to exclude from the image resizing.
Image bottom margin
ImageBottomMargin
Size of the bottom peripheral section to exclude from the image resizing.
Blink
Blink
Allows the object to periodically blink, ignored when the object is not visible.
Colorization mode
ColorizationMode
Set the colorization mode which will be used when applying the selected color to the image.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

MouseDown event
BrowseName
MouseUp event
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal