Histogram chart

Display model or database data in a histogram.
BrowseName
HistogramChart
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Model
Model
Reference to the information model or database from which to obtain the data.
Query
Query
Standard SQL query to filter the data of interest. You can use it to filter data from a database and to filter data obtained from a node-based model. In case of a node-based model, the SELECT * FROM Model part is mandatory, followed by the WHERE clause with which to indicate the search conditions - for example: SELECT * FROM Model WHERE Speed > 40
Label
Label
Visualizes a text.
Value
Value
Value displayed and possibly changed by the user.
Label visible
LabelVisible
Show/hide the scale values.
Value visible
ValueVisible
Show/hide the values of the chart sections.
Value axis visible
ValueAxisVisible
Show/hide the axis of values of the chart sections.
Orientation
Orientation
Horizontal or vertical orientation of the object.
Bar color
BarColor
Sets a single color for the chart bars. If not set, then each bar has a different color.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Methods

Refresh
BrowseName
Refresh
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal