Chart style

Global properties for all project charts.
BrowseName
ChartStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Text color
TextColor
Color of the text to display.
Grid color
GridColor
Axis color
AxisColor
Font family
FontFamily
Font family
Font weight
FontWeight
Font weight
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal