Accordion style

Global properties for all project Accordions.
BrowseName
AccordionStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Border color
BorderColor
Color of the polygon border.
Border width
BorderWidth
Thickness of the object border.
Radius
Radius
Radius of the angles of the objects.
Header background color
HeaderBackgroundColor
Content background color
ContentBackgroundColor
Header icon position
HeaderIconPosition
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal