Search
FactoryTalk Optix Studio Help Center
TwinCAT Tag
BrowseName
TwinCATTag
SuperType
Tag
(Tag)
Properties
Name
BrowseName
DataType
Description
Symbol name
SymbolName
String
Tag name
Memory area
MemoryArea
Memory area
Controller memory location in which to read/write the tags.
Maximum length
MaximumLength
Int32
(string data only) Maximum number of characters in the string.
Byte number
NumByte
UInt32
Number of the byte in the word.
Bit offset
BitOffset
Byte
Bit offset in the word.
Data format
DataFormat
Data format
Encoding
Encoding
Encoding
Decode of memory location contents mode.
Start array index
StartArrayIndex
UInt32
Array update mode
ArrayUpdateMode
Tag array update mode
(Inherited from
Tag
)
Original data type
OriginalDataType
NodeId
(Inherited from
Tag
)
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal