Date and time configuration

Configure the system date and time.
BrowseName
DateTimeConfiguration
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Time synchronization
SynchronizationMode
Time setting mode. Auto = automatic based on the data provided from the remote NTP server; Manual = manual by the user.
Remote NTP server
RemoteNTPServer
(Only if Time synchronization = Auto) Remote NTP server that provides the time.
Date and time
DateTime
Locale date and time
Time zone
TimeZone
Locale time zone, written as a string in IANA format.
Local NTP server interfaces
LocalNTPServerInterfaces
Interfaces though which the system acts as an NTP server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal