PDF generated

The Generate PDF method of a Report object was run.
BrowseName
GeneratePdfCompletedEvent
SuperType
BaseEventType(BaseEventType)

Properties

Name
BrowseName
DataType
Description
Output file
OutputPath
Location in the file system where the PDF file is to be saved (for example, %APPLICATIONDIR%/MyReport.pdf).
Result
Result
Result of the PDF print. 0 = PDF generated successfully; 1 = locale not supported; 2 = failed to process template; 3 = unable to overwrite output file; 4 = unable to generate PDF; 5 = Resource output URI empty or invalid.
Operation ID
OperationId
Locale of the report contents.
EventId
(Inherited from BaseEventType)
EventType
(Inherited from BaseEventType)
SourceNode
(Inherited from BaseEventType)
SourceName
(Inherited from BaseEventType)
Time
(Inherited from BaseEventType)
ReceiveTime
(Inherited from BaseEventType)
LocalTime
(Inherited from BaseEventType)
Message
(Inherited from BaseEventType)
Severity
(Inherited from BaseEventType)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal