RA EtherNet/IP Station

BrowseName
RAEtherNetIPStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Route
Route
Route to the RA EtherNet/IP Controller (for example, 192.168.1.10\Backplane\1)
Timeout
Timeout
Operation code
OperationCode
(Inherited from Communication station)
Tags
(Inherited from Communication station)
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal