Search
FactoryTalk Optix Studio Help Center
OMRON Fins Tag
BrowseName
OmronFinsTag
SuperType
Tag
(Tag)
Properties
Name
BrowseName
DataType
Description
Memory area
MemoryArea
Memory area
Controller memory location in which to read/write the tags.
Data conversion
DataConversion
Data conversion
BCD format
BCDFormat
BCD format
Maximum length
MaximumLength
Int32
(string data only) Maximum number of characters in the string.
Word address
NumWord
UInt32
Address in the memory location in which to read/write the tags.
Bit number
BitOffset
UInt32
Specify the position of the bit in the word.
Flag address
NumFlag
UInt32
Bank number
BankNumber
UInt32
Array update mode
ArrayUpdateMode
Tag array update mode
(Inherited from
Tag
)
Original data type
OriginalDataType
NodeId
(Inherited from
Tag
)
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal