OMRON Fins Station

Object that represents an OMRON Fins PLC.
BrowseName
OmronFinsStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Maximum job size in bytes
MaximumJobSizeInBytes
Maximum size of a transmission of tags from the controller (in bytes). 0 = 1024 bytes (maximum value).
Maximum gap in bytes
MaximumGapInBytes
Maximum distance in bytes between two tags to be part of the same transmission.
Source Network Address
SourceNetworkAddress
Default value = 0. It corresponds to the FINS parameter named Network Address. It can be set to 0 if the PC and all the devices are on the same network. The range of valid values is: 0..127.
Source Node Address
SourceNodeAddress
Default value = 50. It corresponds to the FINS parameter named Node Address. The range of valid values is: 0..254. Usually it corresponds to the last octet of the PLC Ethernet card IP address, i.e. if 192.168.0.54 is the PLC IP address, use 54 as node number.
Source Unit Address
SourceUnitAddress
Default value = 0. It corresponds to the FINS parameter named Unit Address. If the communication is with the PLC CPU, the Unit Number should be 0.
IP address
IPAddress
Unique address to reach the controller on the network
Port
Port
Default value = 9600. This is the number of the TCP port of the device to be connected to. Valid port numbers range from 1 to 65535. Since FINS protocol requires that the source and destination port number be the same, if this parameter is modified, the Local Bound Port parameter should be modified as well and the two values must be equal.
Timeout
Timeout
Maximum wait time in milliseconds to receive a response from the controller.
Optimization type
OptimizationType
Select Datablock when working with consecutive addresses. Mixed Data otherwise.
Operation code
OperationCode
(Inherited from Communication station)
Tags
(Inherited from Communication station)
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal