Memory area

Controller memory location in which to read/write the tags.
BrowseName
MemoryArea

Values

Value
DisplayName
Description
0
CIO area
1
Work area
2
Holding area
3
Auxiliary area
4
Timer
5
Counter
6
DataMemory
7
EM area
8
EM area currentBank
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal