Modbus tag

Object that represents a Modbus PLC tag.
BrowseName
ModbusTag
SuperType
Tag(Tag)

Properties

Name
BrowseName
DataType
Description
Memory area
MemoryArea
Controller memory location in which to read/write the tags.
Maximum length
MaximumLength
(string data only) Maximum number of characters in the string.
Register number
NumRegister
Address in the memory location in which to read/write the tags.
Coil number
NumCoil
Discrete input number
NumDiscreteInput
Bit offset
BitOffset
Position of the memory area register from which to start reading/writing. Position 0 of the Holding register (starting position) corresponds to register 4001.
Array update mode
ArrayUpdateMode
(Inherited from Tag)
Original data type
OriginalDataType
(Inherited from Tag)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal