Search
FactoryTalk Optix Studio Help Center
MELSEC Q tag
BrowseName
MelsecQTag
SuperType
Tag
(Tag)
Properties
Name
BrowseName
DataType
Description
Memory area
MemoryArea
Memory area
Decode of memory location contents mode.
Maximum length
MaximumLength
Int32
(string data only) Maximum number of characters in the string.
Device number
NumDevice
UInt32
Address in the memory location in which to read/write the tags.
Bit offset
BitOffset
UInt32
Encoding
Encoding
Encoding
Decode of memory location contents mode.
Array update mode
ArrayUpdateMode
Tag array update mode
(Inherited from
Tag
)
Original data type
OriginalDataType
NodeId
(Inherited from
Tag
)
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal