MELSEC Q station

Object that represents a MELSEC Q PLC.
BrowseName
MelsecQStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Maximum job size in bytes
MaximumJobSizeInBytes
Maximum size of a transmission of tags from the controller (in bytes). 0 = 128 bytes (maximum value).
Maximum gap in bytes
MaximumGapInBytes
Maximum distance in bytes between two tags to be part of the same transmission.
IP address
IPAddress
The IP address of the controller Ethernet module.
Port
Port
Set it to the Local station Port No. of the TCP or UDP connection configured in the PLC Ethernet module. Please note that the decimal format must be used. When the TCP/IP protocol is selected (see Driver Settings) the default value for the Server Port is 0, while if the UDP/IP protocol is selected, the default value is 5000.
Timeout
Timeout
Maximum wait time in milliseconds to receive a response from the controller.
Network Number
NetworkNumber
Set it to the Network No. of the controller Ethernet module.
PC Number
PcNumber
Set it to the Station No. of the controller Ethernet module.
Number base
NumberBase
Numerical base for addressing the controller memory.
Operation code
OperationCode
(Inherited from Communication station)
Tags
(Inherited from Communication station)
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal