Event logger

Records the properties of one or more event types of interest generated by a specific node and/or by its child nodes, or by any node in the project, and stores them in a database.
BrowseName
EventLogger
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Enabled
Enabled
Enable/disable the recording of events.
Locales
Locales
Locales of interest for storing translations of LocalizedText data in the database, typically the descriptions of the events. Each locale has an additional column in the database for each localized property. If empty, the locales are those expected by the project (Locales property of the project root node).
Database
Store
Database in which to store the events data.
Event configurations
EventConfigurations
Event configuration collection of objects. If empty, record events generated by any project node.
Paths to event fields
EventFieldPaths
Event arguments
EventArguments
Event fields to log
EventFieldsToLog
Properties to record of the different events of interest.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal