CODESYS Station

BrowseName
CODESYSStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Gateway IP
GatewayIP
IP address of a valid CODESYS Gateway available in the network; usually, the IP address of the controller.
Port
Port
TCP/IP port used to connect with the controller. The property has meaning only for Version 2.3 controllers; if using other controller versions the property will be disregarded. You can obtain the value from the CODESYS PLC Programming Environment: From the On line menu, select Communication Parameter.
Device Name / Address
PLCAddress
The CODESYS Controller Device Name or its IP address. The IP address can refer to the same machine that runs the driver using the local IP address or localhost.
Timeout
Timeout
Maximum wait time in milliseconds to receive a response from the controller.
PLC version
PlcVersion
Controller version. Either Version 2.3 or Version 3.
Endianness
Endianness
Byte ordering in accordance with the architecture of the processor with which the communication is established.
Login to PLC
LoginToPlc
Default value: False. Some special devices can require or not a login on the PLC. Leave the default value if not specified othervice in the device documentation.
Protocol
Protocol
Default value: TCP IP L2 ROUTED. Available values: TCP IP L2 ROUTED, TCP IP L2, TCP IP L4. Some devices may require a special communication protocol. Leave the default value if not otherwise specified in the device documentation.
Communication Buffer Size
CommunicationBufferSize
Communication buffer dimension. Valid only for 2.3 controllers version. Default value: 0, which means automatic management. On the target, verify the correct setting.
Operation code
OperationCode
(Inherited from Communication station)
Tags
(Inherited from Communication station)
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal